The KP200 series utilises a built-in rechargeable battery that can be used to unlock the drive first without using any software, and then plug it into any device that supports USB Type-A or USB Type-C mass storage device. This gives users the most flexibility across different platform types and operating systems.
With the Multi-PIN option (Admin/User), the keypad can be used to set up an easy-to-remember but hard-to guess alphanumeric PIN for the Admin or User accounts. Admin can restore a User PIN and provide access to the drive should the User PIN be forgotten, or if the drive is locked after reaching the maximum of 10 User login attempts. With both Admin and User PINs enabled, KP200 will lock the User PIN after 10 failed login attempts; if the Admin PIN is entered incorrectly 10 times in a row, brute force attack protection will crypto-erase the drive, destroy the data forever, and reset it.
The drive also provides two levels of Read-Only (or Write-Protect) modes – a Global mode that can be set by Admin, and a session-only mode that can be set by User. Read-Only modes can protect the drive from malware on untrusted systems. In addition, Admin can load content and set Global Read-Only mode, so that User can access the data but not make any changes.
Fast dual-channel performance is offered on KP200 drives with 512GB and on KP200C drives with 64GB-512GB capacities.