ROG ZEPHYRUS G14

Performance Meets Precision

Enjoy effortless Windows 11 Pro gaming and creating experience with up to an AMD Ryzen™ 9 8945HS processor
Game and create with up to an NVIDIA® GeForce RTX™ 4070 Laptop GPU
ROG’s first 3K OLED 120Hz/0.2ms Nebula Display, with VESA DisplayHDR True Black 500 support
Ultra slim 1.59cm 1.5kg 14” Premium aluminum chassis
ROG Intelligent Cooling, Tri-fan technology, liquid metal, improved heatpipes and 2nd Gen Arc Flow Fans™
Brand new feature Slash Lighting

The New Era

Power, precision, and elegance define the 2024 Zephyrus G14. Thinner and sleeker than ever before, the Zephyrus G14 still has the same sense of style and individuality that has always set it apart from the crowd. Featuring an all-aluminum CNC-machined chassis, this laptop is the perfect blend of performance and style.

NVIDIA® GeForce RTX™ 4070 Laptop GPU in 1.59cm CNC Aluminum Chassis

The Future is Here

Game and create with ease on this Windows 11 Pro powered machine. Featuring up to an AMD Ryzen™ 9 8945HS processor and up to NVIDIA® GeForce RTX™ 4070 with AI accelerators, this 14-inch machine can easily handle the latest games and cutting-edge creative software alike. Whether you’re in a video call, editing a video, or in a next generation game, AI accelerators are working tirelessly behind the scenes to improve your experience. GeForce RTX GPUs feature specialized AI Tensor Cores that deliver cutting-edge performance and revolutionary capabilities.

Windows 11 Pro

Besturingssysteem
Up to

AMD Ryzen™ 9

8945HS
Up to NVIDIA® GeForce

RTX™ 4070

Laptop GPU

Gaming

Creating

Productivity

Beyond Fast

The Zephyrus G14 is built from the ground up for gamers — and, of course, game developers. Equipped with up to an NVIDIA® GeForce RTX™ Laptop GPU, the G14 can run all the latest games and game development engines. Plus, with game-changing features like DLSS 3.5 with Frame Generation, and the latest ray tracing enhancements, this machine offers unprecedented realism in modern titles. NVIDIA® Advanced Optimus support allows for seamless transitioning between low power and low latency modes the moment a game is launched, and with a max TGP of 90W, the GPU is always allowed to fully flex its silicon muscles.
Up to NVIDIA® GeForce
GeForce RTX 4070
Laptop GPU
Max TGP
90W
with Dynamic Boost
NVIDIA®
Advanced Optimus
Up to
265 AI TOPS
(4070 Laptop GPU@65W)

Your Ideas, Accelerated by NVIDIA Studio

Creativity that’s all in. NVIDIA Studio is your creative advantage with state-of-the-art RTX GPUs that power the world’s premiere creative apps. Real-time ray tracing delivers hyper-realistic graphics and the Studio suite of exclusive AI-assisted tools take your ideas and designs from concept to completion, faster. With NVIDIA Studio Drivers, your digital canvas is always up-to-date with maximum stability and performance, so you can focus on your next big idea.

Get next-level AI performance on GeForce RTX

Discover the RTX AI advantage. Built for the era of AI, GeForce RTX™ and NVIDIA RTX™ GPUs feature specialized AI Tensor Cores that deliver cutting-edge performance and next-gen capabilities. From enhanced creativity and ultra-efficient productivity to blisteringly fast gaming, the ultimate in AI power on Windows PCs is on RTX.


Soar Past the Limit

With 8 cores and 16 threads, the AMD Ryzen™ 9 8945HS processor is ready to power all of your games and creative applications with ease. Built on the Zen 4 architecture, this cutting-edge chip is the perfect blend of performance and power efficiency that make it ideal for an ultra-portable laptop like the Zephyrus G14.
Up to
AMD Ryzen™ 9 8945HS
AMD Ryzen™ AI
Up to 39 TOPs
8
Cores
16
Threads

Advance Your PC Experience with AMD Ryzen™ AI and Windows Studio Effects

The Zephyrus G14 supports AMD’s all new Ryzen AI™*. These dedicated hardware AI accelerators built into the silicon, combined with a suite of software, free up CPU and GPU resources to ensure optimal performance in all-new experiences. From hand gesture detection to eye gaze correction and super resolution upscaling, your video calls will feel more lifelike and seamless than ever.

*AMD Ryzen™ AI is available on select AMD Ryzen™ 8000 Series processors.


 

Automatic Framing

Automatically pans and zooms the video to focus on you as you move.

Eye Contact Correction

An effect to compensate for eyes looking away from the center of the camera.

Advanced Background Effects

New, high quality background blurs enabled by AI.

AMD XDNA - AI Engine​

AMD XDNA is a spatial dataflow NPU architecture consisting of a tiled array of AI Engine processors. Each AI Engine tile includes a vector processor, a scalar processor, and local data and program memories. Unlike traditional architectures that require repeatedly fetching data from caches (which consumes energy), AI Engine uses on-chip memories and custom dataflow, to enable efficient, low power computing for AI and signal processing.
Software Programmable
The AMD NPU is programmable and compiles in minutes. It also leverages a library-based design to simplify the workflow for ML framework developers.
Deterministic
The AMD NPU includes dedicated instruction and data memories, as well as dedicated connectivity paired with DMA engines for scheduled data movement using connectivity between AI Engine tiles.​
Efficient
The AMD NPU delivers greater compute density compared with traditional architectures and drives exceptional power efficiency.​
Scalable
The AMD NPU is architected as 2D arrays consisting of multiple AI Engine tiles, enabling scaling from 10s to 100s of AI Engine tiles in a single device, servicing the compute needs of a breadth of applications.​​

Help is always at hand


Copilot in Windows 11 complements your capabilities and creativity with intelligent assistance and relevant answers.

*Screen simulated, subject to change. Feature availability and rollout timing may vary.

Get time saving assistance
Summarize emails with Copilot in Windows 11

Get the answers you need
Get personalized guidance with Copilot in Windows 11

Control the settings you want
With Copilot in Windows 11

*Copilot in Windows (in preview) is rolling out gradually within the latest update to Windows 11 in select global markets.

OLED is Here​

For the first time on an ROG laptop, enjoy the ultra-fast response times and incredible contrast ratios that are only possible with OLED technology. This ROG Nebula panel also boasts a 3K resolution, giving it incredible pixel density on a 14-inch screen, with a 120Hz refresh rate that makes all of your games look silky smooth. With 100% coverage of the DCI-P3 color space, a delta E color accuracy of less than 1, and VESA HDR True Black 500 certification, prepare to be immersed in HDR content so lifelike that the screen melts away.

*Average tested result in MyASUS / Armoury Crate Splendid Display P3 and sRGB color gamut: Delta E < 1, +/- 0.5, and may vary by specification. Please note that the actual performance also may vary under different test procedures, equipment and patterns.
Fast

Leading OLED panels with NVIDIA G-SYNC

OLED displays have an ultrafast 0.2ms response time, which ensures smoother fast-paced action scenes, low-latency gameplay, and subtle details like blur-free text scrolling.

0,2 ms

Response time


Bright

1,000,000:1 Ultra-High Contrast Ratio

OLED displays have millions of light-emitting diodes (LED), and unlike traditional display technologies, they can turn each pixel on and off individually. Because of this, OLED panels can achieve pixel-perfect black levels, resulting in extreme contrast ratios like 1,000,000:1. This true black allows for images that appear bright and punchy without feeling washed out, ensuring you never miss an enemy hiding in the shadows. HDR has never looked this good.

1 000 000:1

Contrast Ratio
Vivid

3K Resolution

Enjoy incredibly vivid scenes thanks to the added visual fidelity offered by a 3K resolution. With a higher pixel density than 1440p, 3K displays allow the true vibrance of both still images and video content to truly shine.

3K Resolution

NVIDIA G-SYNC Technology

Nothing breaks in-game immersion like stuttering and tearing. GPUs render frames at variable rates, but displays usually refresh at a constant clip, so they can get out of sync, causing visible hitching and artifacts that pull you out of the action. ROG is proud to introduce the first-ever OLED display in a laptop capable of using NVIDIA® G-SYNC, which allows the refresh rate of the display to synchronize with the GPU’s frame rate to eliminate visual tearing, minimize stuttering, and reduce input lag.

Dolby Vision® Technology

Scene to scene, frame to frame, Dolby Vision makes media look better. The technology improves on standard 4K high dynamic range (HDR) video, dynamically adjusting visuals to make every image in front of you richer, brighter, and livelier. Creators can film and edit their streams, videos, and other content in a format commonly used by industry professionals.

Pantone® Color Validation

Each IPS-level display is factory-calibrated to ensure that colors are accurate to the Pantone® palette. Artists, designers, and content creators can add high-quality content to their portfolios and enjoy richer gaming visuals all on the same machine.

100% DCI-P3 Color Coverage

While the sRGB color space is the standard for most digital visuals, it only represents about 75% of the DCI-P3 spectrum used for professional filmmaking. Displays with complete DCI-P3 coverage offer a wide color gamut for more vibrant images, and with a Delta E of less than 1*, the Zephyrus G14’s display lets you experience films and other media exactly the way they were meant to be seen.

*Average tested result in MyASUS / Armoury Crate Splendid Display P3 and sRGB color gamut: Delta E < 1, +/- 0.5, and may vary by specification. Please note that the actual performance also may vary under different test procedures, equipment and patterns.

Cool, Calm, Collected​

ROG Intelligent Cooling is a suite of components that work together in harmony to keep our high-performance laptops cool and quiet. The Zephyrus G14 boasts some never-before-seen additions to ROG’s list of cooling technologies, including improved heatpipes, Tri Fan Technology, 2nd Generation Arc Flow Fans™, and a redesigned high-efficiency air outlet. Taken together, these systems keep the machine operating at its peak while staying quieter than ever.

Tri-Fan

Technology

2nd Gen

Arc Flow Fans

0db

Ambient Cooling

Liquid Metal

Keys to Mastery

The trackpad and keyboard are critical for controlling your laptop, so we spared no expense with the design of the Zephyrus G14. Despite being just a 14-inch device, the G14 boasts a large 16:10 aspect ratio trackpad for superior typing, precision scrolling, and fluid gaming. We’ve also increased the keycap size by 12.24% for smoother typing as well, thanks to extra rigidity from the CNC machining. An extra long 1.7mm travel distance gives the keyboard a premium typing feel, and with a lifetime of 20 million presses, it’s a perfect long-term partner.

Premium Glass Power Key 

Windows Hello

An infrared camera ensures seamless unlocking with Windows Hello support, even in low light conditions.

Aura Sync

Aura Sync support allows you to easily pair and color coordinate all of your ROG RGB equipped peripherals.

Stealth Hinge Design

12.24% Larger Key Cap

Sleek Design

The new Zephyrus G14 catches your eye the moment you see it. Precision CNC-machined from aluminum alloy, this high strength material accepts complex shapes and also looks absolutely gorgeous after being anodized in either Eclipse Gray or the all-new breathtaking Platinum White colorway. The sleek chassis and matte finish of the Zephyrus G14 simply beg to be touched.

CNC Machined
Precision Craftsmanship
100%
Aluminum Alloy
Stealth Hinge
Design

A Slice of Brilliance

The Zephyrus G14 introduced the world to AniMe Matrix™, a robust LED array that made every G14 stand out from the crowd. In 2024, the G14 once again breaks the mold, debuting an all new lighting design: the Slash Lighting array. A bold streak across the lid of the machine, Slash Lighting is an evolution of the elegance and individuality that make Zephyrus so unique. It retains the customization of its predecessor, with a design inspired by sci-fi and contemporary art.

15
Preprogrammed Animations
Sonic Match
Notification

Pump Up The Volume

Get lost in the music with the new and improved woofers on the Zephyrus G14. With a staggering 252% volume increase and an ultra-low bass frequency of 100Hz, the G14 produces clear and vibrant sound that you wouldn’t expect from an ultra-slim 14-inch machine. Whether you’re vibing to your favorite podcast or saving the world in the latest games, the Zephyrus G14 is ready to pump up the volume.

6
Speakers
Dual side
Woofers
252%
Volume Increase
125%
Woofer Unit Increase
100Hz
Bass Low Frequency

All day power

The Zephyrus G14 has always been defined by its portability, and the 2024 model is no exception. This incredible gaming machine is a true thin-and-light, weighing in at just 1.5kg, with some models measuring as low as 1.59cm thick. Paired with a 73Wh battery that supports fast charging from 0-50% in just 30 minutes and support for Wi-Fi 6E wireless networking, the Zephyrus G14 is the ultimate gaming and productivity machine for those on the move.


73Wh

Battery

1,5KG

50% in 30min

That mobility continues with fast charging support that can juice up the G14 from 0-50% in just 30 minutes.

Wi-Fi 6E

With full support for the Wi-Fi 6E standard, the G14 can enjoy broadband level connections, even in congested networks.

1,59cm

Despite its svelte and supremely portable chassis, the G14 offers all of the connectivity to enable your workflow or the battlestation of your dreams. Dual USB-C ports, both of which support display output, and one that supports both Power Delivery 3.0 and DisplayPort 1.4 make the very most of this versatile connector. For your other peripherals, dual USB 3.2 Gen2 Type-A ports expand connectivity even further. For quick file transfers or extra storage, a dedicated UHS-II MicroSD card reader stands ready.

OLED Care

ROG OLED laptops come with an ROG-exclusive OLED Care mechanism that’s proven to protect your display. Image persistence, or burn-in, on an OLED display can occur if a static high-contrast image is displayed for a prolonged period of time. To avoid this, when your ROG laptop is idle for over 30 minutes, our specially designed Pixel Refresh feature kicks in.

Armoury Crate

When you want to tweak settings, monitor temperatures, or tinker with your laptop, Armoury Crate is your command center. Real-time monitoring allows you to see what your GPU, CPU and memory are doing. RGB can be adjusted on a game-by-game basis with Aura Sync. Fan and power profiles allow you to change the acoustics, power delivery, and thermal characteristics of the laptop on the fly. And exclusive game deals keep your library topped off at all times.