Alienware Aurora Gaming Desktop

Optimised for all gamers

The Alienware Aurora Gaming Desktop features incredible performance boosts and focuses on reducing acoustics while maintaining airflow. Making it a perfect gaming system for any setting with purpose-built legend 3 design.

Top-tier gaming versatility

The Alienware Aurora is engineered for exceptional performance with a streamlined, minimal design. This generation of Aurora desktops focuses on reducing acoustics while maintaining airflow, making it a perfect gaming system for any setting.

Legend perfected

Modern design with a matte "basalt black" finish in an optimised chassis with customisable AlienFX lighting zones, including the striking stadium lighting. Available with a Clear Side Panel for showing off the internal components, with the elevated Legend 3 industrial design.

Purpose-built design

HEXAGONAL SIDE VENTS

An array of hexagonally shaped vents enables passive air intake supporting graphics performance and quieter acoustics.

STREAMLINED DESKTOP

Our Legend 3 design is echoed by the overall compact and functional size of the system, which is about 40% smaller by volume than the previous design and up to 53% smaller than the Area-51.

CLEANER CABLE MANAGEMENT

Seamless internal cable management reduces obstruction of airflow and keeps thermals efficiently managed.

FRONT I/O FLEXIBILITY

High performance front ports enable great connectivity and two of the USB ports include PowerShare technology which lets you easily power your favourite external devices even while the system is shut down.

Intentional thermal strategy

Our design prioritises airflow efficiency and improved acoustics by introducing larger passageways and optimised internal cable management resulting in 20% quieter operation, on average, and 7% lower temperatures compared to the Aurora R15¹. This approach — combined with liquid cooling CPU option — contributes to an incredibly smooth gaming experience.

Game cool and quietly

Central to the Aurora thermal strategy is the increase in its ventilation's total surface area. This increase is the driving force behind the desktop's efficient airflow, cooling and acoustics.

Optimised airflow strategy

The side hexagonal array, top surface exhaust, and the front stadium intake all provide significantly larger pathways for ambient air to enter and heat to be exhausted.

240mm heat exchanger

The 240mm heat exchanger, available on the CPU liquid cooling, heightens thermal resistance, ensuring temperatures stay consistently low during longer gaming sessions.

Updated heat exchanger fans

Revamped 240mm heat exchanger fans are designed to be smoother in angle and shape, making airflow more efficient with less fan noise.

Game changing graphics

Step into the future of gaming and creation with the NVIDIA® GeForce RTX™ 50 Series, powered by NVIDIA Blackwell architecture. Designed to push boundaries, this GPU lineup delivers unparalleled AI performance and jaw-dropping graphics fidelity — perfect for those who demand the extraordinary.

Ray Tracing Redefined

Experience cinematic realism with full ray tracing, brought to life by fourth-gen RT Cores. From stunning light reflections to intricate shadows, your in-game world looks better than ever.

AI-Boosted Gameplay

Unleash next-level speed and responsive gaming with DLSS 4. Achieve ultra-smooth frame rates with Multi Frame Generation and enhanced Ray Reconstruction powered by fifth-gen Tensor Cores.

Competitive Advantage

Compete faster with NVIDIA® Reflex 2 technology featuring Frame Warp, which further reduces latency based on the game’s latest mouse input.

Unparalleled Video Playback

The RTX 50 Series redefines how you enjoy your favourite movies, shows and videos. With advanced AI-powered upscaling and buttery-smooth playback, immerse yourself in vibrant colors, stunning clarity and flawless streaming.

Immersive Entertainment

Rethink how you stream, chat or create content with NVIDIA Broadcast’s advanced AI enhancements. Clear your audio, upgrade your video, and craft your AI-powered home studio effortlessly.

Marathon gaming unlocked

All Auroras are equipped with our 12-phase voltage regulation design. This high-performance technology ensures clean energy is consistently available, unleashing the top-level power of up to Intel® Core™ Ultra processors as you game, livestream, and multi-task for hours on end. For more demanding experiences, the new Ultra K-Series processors are unlocked and can be overclocked².

CPU

Ensures everything runs smoothly and as expected; like controlling non-player characters, calculating realistic physics, translating a button press into an action, and triggering sound effects at the right time in the game.

NPU

Dedicated AI accelerators provide intelligent performance across gaming, creation and streaming apps where AI capabilities are possible.

More performance, quicker multitasking

Upgradable parts enable gamers to tailor their experience and expand the lifespan of their PC.

Gen5 PCIe performance

The Alienware Aurora includes the Intel® Z890 chipset with three PCIe slots. The primary Gen5 PCIe slot³ provides x16 physical and electrical lanes devoted to maximum performance.


Faster multitasking

Load large games and handle intensive tasks with up to 64GB of DDR5 XMP memory.


Two PCIe NVMe M.2 slots

Enabling up to 8TB of total solid state storage space.


Available 3.5” hard disk drive

To store, run and archive any games, files, or applications.


Advanced Networking

Made possible with Wi-Fi 7⁴, 2.5 Gbps ethernet, enabling the best wired and wireless connection.

Alienware Elite Care

Next-Level Gaming Support

We know gaming. Talk directly to our elite Alienware support experts, anytime⁵.

Support Essential

Accidents happen. Alienware Elite Care includes Accidental Damage Service for fast and seamless repairs due to drops, spills and electrical surges⁶.

SupportAssist Technology

Your personal wingman to keep you gaming at peak performance – predicting and resolving issues before they occur⁷.

Total command

Alienware Command Centre software allows you to create and edit AlienFX lighting across the ecosystem, choose and monitor your performance mode across distinct power states, and create custom gaming profiles for your whole library.

Expressive gameplay

Show off your gaming style by customising AlienFX lighting across your Alienware ecosystem with millions of colour combinations at your disposal.

Performance presets

Choose and monitor performance across distinct power states - quiet mode, balanced mode, and performance mode - according to your gaming preferences.

Game your way

Play through every game exactly how you want by creating customised gaming profiles for your whole library.

All for play and play for all

Game with the graphics you need, with the people you want, with the peripherals you prefer.


Whatever parts you pick, Windows 11 has the software to make the most of them to deliver the high framerate, high resolution experience you desire.


Chances are that the game you want to play is compatible on Windows. With PC Game Pass, you can have even more to try—especially the latest titles on release day⁸.

Get your game on

Play hundreds of PC games, and day one blockbusters with your new Alienware PC and PC Game Pass — including EA play. With new games added all the time, there’s always something new to play⁹.

Ports and slots

Front Ports

  1. 1x Global headset jack
  2. 2x USB 3.2 Gen 1 (5 Gbps) Type-A port
  3. 1x USB 3.2 Gen 1 (5 Gbps) Type-A port with PowerShare technology
  4. 1x USB 3.2 Gen 2 (10 Gbps) Type-C© port with PowerShare technology

Rear Ports

5. 1x Line In

6. 1x SPDIF Digital Output (TOSLINK)

7. 1x Line Out

8. 1x USB 4 (20 Gbps) Type-C© port

9. 2x USB 3.2 Gen 1 (5 Gbps) Type-A port

10. 2x USB 2.0 Type-A ports with Smart Power technology

11. 1x USB 3.2 Gen 2 (10 Gbps) Type-C© port

12. 1x RJ-45 Killer™ E3100G 2.5 Gigabit Ethernet

Dimension and weight

Including Rear pull bar and rubber foot

  1. Height: 418.00 mm (16.46")
  2. Width: 197.00 mm (7.75")

Including Rear pull bar and rubber foot

3. Depth: 458.40 mm (18.05")

Maximum weight: 15.37 kg (33.89 lb)¹⁰

Regulatory Product Compliance & Environmental

Dell Technologies is committed to compliance with the laws and regulations in each country into which the company ships it's products. Dell products are designed and tested to meet the appropriate worldwide standards for Product Safety, Electromagnetic Compatibility, Ergonomics, and other regulatory compulsory requirements when used for their intended purpose.


In addition, Dell products are developed with design for the environment in mind. Our environmental stewardship program drives conservation of product energy consumption, develops methods to reduce or eliminate materials for disposal, prolongs product life span, and provides effective and convenient equipment recovery solutions.

1. Based on internal analysis, June 2023, using identical components. Performance may vary.

2. Overclocking for 14th Gen Intel® Core™ K-series processors can be managed in the system's BIOS.

3. Two additional Gen3 x4 PCIe slots are available but may not be accessible with most graphics options.

4. Wi-Fi 7 certified products will roll out in accordance with the Wi-Fi Alliance certification schedule throughout 2024. Wi-Fi 7 requires the latest Wi-Fi Alliance certification, Windows HLK certified device driver, hardware update, supported Windows OS version and compatible router. Wi-Fi 7/ 6E connectivity (6 GHz) with Windows 11 is limited and will leverage prior generation of Wi-Fi 6E/ Wi-Fi 6 speeds until drivers are available and hardware adoption increases. Ubuntu OS will not support Wi-Fi 7 and will operate on Wi-Fi 6E/6 speeds when configured for Wi-Fi 7. Router requires a separate purchase. Wi-Fi 7/ 6E (6 GHz) connectivity is only available in select locations. Check availability with your service provider. The Bluetooth wireless card version may vary depending on the operating system that is installed on your computer.

5. Alienware Elite Care requires a separate purchase. Designated tech support - Availability may differ outside of North America and is limited to commercially reasonable efforts. For more information, visit www.dell.com/support to determine how to get more assistance.

6. Accidental damage coverage excludes theft, loss, and damage due to fire, flood, or other acts of nature, or intentional damage. Customer must return damaged unit. Limit of 1 qualified incident per contract year.

7. For supported system and requirements, please refer to our user guide (SupportAssist for Home PCs version for personal use) or administrator guide (SupportAssist for Business PCs version for PC fleet management) and select supported PCs. Proactive and predictive capabilities depend upon your active service plan and Dell Technologies business rules. For ProSupport Suite for PCs capabilities view our administrator guide and select Connect and manage capabilities and Dell service plans. For Premium Support Suite for PCs capabilities view the user guide and select SupportAssist capabilities and Dell Services plans.

8. Subscription sold separately.

9. Credit card required. Subscription continues automatically at regular monthly price unless cancelled. Subject to xbox.com/subscriptionterms. Digital Direct: Your digital content will be delivered directly to your device during set up; no codes required.

10. Weights vary depending on configuration and manufacturing variability.