Dell Memory Upgrade - 16 GB - 2Rx8 DDR4 RDIMM 3200 MT/s

Dell Part AA799064


Random Access Memory (RAM) is a type of hardware that your computer uses to store information. Adding memory is one of the most cost-effective ways to improve your computer's performance.

Media

Why should I buy a Dell Upgrades over a third-party part?

Tested and Verified Tier-1 OEM-Grade Parts

Ensure compatibility with Dell servers, storage and networking.

Ease of Installation

Save time with Dell Upgrades that are shipped as kits with the necessary hardware and firmware.

Secure Supply Chain Focus

Protect system data and integrity with parts sourced from a secure supply chain.

Dell Tech Support and Warranties

Preserve Dell technical support and warranties - which do not support systems with third-party upgrades.

Compatibility

This product is compatible with the following systems:

  • PowerEdge C6525
  • PowerEdge R450
  • PowerEdge R650xs
  • PowerEdge R6515
  • PowerEdge R6525
  • PowerEdge R7515
  • PowerEdge R7525
  • PowerEdge T550
  • PowerEdge XR2
  • PowerEdge XR4510c
  • PowerEdge XR4520c
  • PowerVault NX3240
  • Precision Workstation 5820 Tower
  • Precision Workstation 7820 Tower
  • Precision Workstation 7865 Tower
  • Precision Workstation 7920 Tower
  • Precision Workstation R7920
  • Precision Workstation R7920 XL
  • Precision Workstation T5820XL Tower
  • Precision Workstation T7820XL Tower
  • Precision Workstation T7920XL Tower

Memory DIMM Types

With more memory, the faster that data and instructions can be read, written, and performed by the server.

There are three types of memory DIMMS for servers available. These DIMM types cannot be mixed in a single system, you must select the type of DIMM appropriate for your workload at the type of purchase.
  • Unbuffered DIMM: UDIMM, an unbuffered, low density, low-latency DIMM that doesn't include a register or buffer chip. UDIMMs are generally used in applications requiring the lowest possible latency.

  • Registered DIMM: RDIMM, a registered DIMM that provides high signal integrity -- performing parity checking to detect improper addresses or commands -- and increased performance for heavy workloads.

  • Load reduced DIMMs: LRDIMM, uses a buffer to reduce memory loading to a single load on all DDR signals, allowing for greater density

Memory Tests

  • Burn-in: Powered stress testing (i.e. increased temperature) to remove weak components.

  • Component Test: Memory vendor-specific diagnostic tests performed at DRAM component level to ensure functionality.

  • Module Test: Memory vendor-specific diagnostic tests performed at DIMM level to ensure functionality (with all DRAM components already mounted on DIMM PCB).
Random Access Memory (RAM) is a type of hardware that your computer uses to store information. Adding memory is one of the most cost-effective ways to improve your computer's performance.

Memory offered now may differ in speed from the original system memory but has been qualified to work in the system. When mixed, the memory will perform at the lowest speed populated or the highest speed allowed by the system